Forty Siemens’ Bridges Electric™ Vector™ automated, group-operated air break switches are included in Austin Energy’s Smart Grid pilot project. The Vector™ switches are capable of sensing voltage and current and are remotely controlled through supervisory control and data acquisition (SCADA) in both normally closed and normally open points within the distribution feeders. All switch operations are remotely controlled by a SCADA operator and/or master system software, thereby eliminating the need to operate the devices from the control cabinet. The controller is fully capable of performing automatic sectionalizing operations.
This pilot project plays an integral part in the functional testing of the intelligent grid scheme planned by Austin Energy and its partners. Highlights of the Austin Energy pilot project include:
Siemens’ Bridges Electric™ RCMS™ remote current monitoring system for fault current detection
Three-phase voltage sensing on both the source and load sides of the switch for use on normally closed and open points within the distribution system
Remote supervisory control achieved via a programmable remote terminal unit via DNP 3.0, Level 2 and radio communication.
Necessary current and voltage sensing cables, motor control cable, antenna and antenna cable are also provided by Siemens as part of an integrated solution that allows for a "plug-and-play" approach as well as a reduction in the utility's installation costs.
Powering the Texas capital, Austin Energy is the nation’s ninth largest community-owned electric utility serving 388,000 customers and a population of more than 900,000. The utility manages over 2,600 megawatts of generation comprised of a diverse mix of nuclear, coal, natural gas and renewable energy sources.
This is Austin Energy’s initial foray into automation, but this municipal utility is certainly no stranger to progressive energy programs. Austin Energy created the top performing renewable energy program in the nation. Owning the nation’s first and largest green building program, the utility is home to one of the nation’s most comprehensive residential and commercial energy efficiency programs.
"Siemens understands that a Smart Grid is more than smart meters -- it includes integration of renewables, making the transmission network more intelligent as well as automating the distribution network," said Muhammad Sohail, vice president of the High Voltage Products business unit of Siemens Energy, Inc. "We're proud to be the only supplier in the world with products and solutions along the entire energy conversion chain, including those necessary to ensure a successful Smart Grid project."
Siemens provides Smart Grid solutions along the entire energy conversion chain from planning and consulting to the products and services required to enable the grid to operate intelligently. And Siemens also incorporates solutions for commercial and industrial applications as well as smart homes including building automation, IT systems integration, advanced lighting technology and energy efficient appliances for a comprehensive Smart Grid solution.
The Siemens Energy Sector is the world’s leading supplier of a complete spectrum of products, services and solutions for the generation, transmission and distribution of power and for the extraction, conversion and transport of oil and gas. In fiscal 2008 (ended September 30), the Energy Sector had revenues of approximately EUR22.6 billion and received new orders totaling approximately EUR33.4 billion and posted a profit of EUR1.4 billion. On September 30, 2008, the Energy Sector had a work force of approximately 83,500. Further information is available at: www.siemens.com/energy.